Hello there, here is the thing
Basically I have a C1D2 (Class 1 División 2, hazardous location) engine, the engine comes with the Customer interface harness where the signals are separated as Incendive and NON incendive which meets the C1D2
The J1939 is a non incendive signal.
That means I cannot interface the J1939 of the engine with the Danfoss controller Can bus directly. In other words if I want to do that I need a barrier or so.
the question is, does any one have dealed with this? did you find any barrier to interface the CAN BUS?
Regardsless of the Engine RPM control I want to monitor the engine parameters in a safe area.
I have a controller in a N7 box at the equiment that also monitors pressures from Intrinsically safe sensors
the other question could be for the Danfoss guys, is the CAN BUS of the controller a non incendive signal?
Here is the definition of non incendive signal
"equipment having electrical/electronic circuitry that is not capable, under normal operating
conditions, of causing ignition of a specified flammable gas-, vapor-, dust-air mixture fibers or
flyings due to arcing or thermal means"
in the specifications of the controller does no say anything related that is wy I am not sure
I appreciate any feedback
Thanks
![Cry :'(](https://www.plus1forum.danfoss.com/Smileys/SoLoSMiLeYS1/cry.gif)