Author Topic: PVEA Error signal  (Read 4110 times)

Offline SorenHPedersen

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +0/-0
PVEA Error signal
« on: November 16, 2013, 04:36:32 PM »
Hi

I 'am new using the Sauer Danfoss controllers and have just made my first hardware setup using a MC088 and 9 PVEA valves. But for one PVEA my Error signal jumps to about 9V when I connect it to my input "C1p07_DigIn".
If I leave the input not connected the PVEA still works. It's the same if I switch PVEA's
Any idea?

Søren
 

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: PVEA Error signal
« Reply #1 on: November 27, 2013, 04:04:05 PM »
Hi Søren,

Sorry for the late reply.

If you are still facing issues with this, I suggest you send your application (as a P1P) into helpdesk (plus+1helpdesk@danfoss.com), together with a detailed description (screenshots are also always very good), then we can have a look at it.


Best regards
Daniel
PLUS+1® HelpDesk
PLUS+1® Help Desk Team