Author Topic: Driving a Diesel engine speed with Plus One?  (Read 5164 times)

bgtwuk

  • Guest
Driving a Diesel engine speed with Plus One?
« on: January 19, 2013, 12:28:02 PM »
Has anyone had success driving the VSG input (V14) on a DEtroit diesel?

It looks for a voltage signal between .4 and 4.5 volts.

When I send a value using a PVE output (config 6), the engine speed is never stable.

I am using a voltage output joystick.

BGTWUK

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: Driving a Diesel engine speed with Plus One?
« Reply #1 on: January 21, 2013, 01:21:03 PM »
I've always use the J1939 CANbus to drive engine rpm. PGN-0