Author Topic: Communication error  (Read 5929 times)

pgrosshart

  • Guest
Communication error
« on: October 18, 2011, 01:06:02 AM »
I new... the CG150 can't find the DP200 attached, does it need a termination resistor to work?

bgtwuk

  • Guest
Re: Communication error
« Reply #1 on: October 18, 2011, 03:11:30 AM »
Often, Yes.

It is beat to add to your breakout cable that you use to power up the module.

Good luck.

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: Communication error
« Reply #2 on: March 30, 2012, 03:48:27 AM »
you may have solved it by now,

but you need to create your CAN bus line if working only with the DP200 and your laptop. the termination resistor used to be added when working with a machineĀ“s ECU and the DP 200.

Regards