Author Topic: Servo Valve requiring +/- 15v  (Read 7077 times)

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +2/-0
    • Trebro Turf Equipment
Servo Valve requiring +/- 15v
« on: December 11, 2017, 04:13:22 PM »
Hello,

I would like to try using a Servo Valve in our application for better spool response time and accuracy. Our application requires very swift and accurate movement (move traverse 5-6 ft., over and back in roughly 2 seconds).

I have yet to find a servo valve that does not have an input signal of +/- 15v, which I am pretty sure a Plus+1 Controller is not capable of.

Has anyone controlled a Servo Valve (or something similar) with a Plus+1 Controller?

Is there external hardware I can incorporate to make this happen?

Thanks,

Jake

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: Servo Valve requiring +/- 15v
« Reply #1 on: December 15, 2017, 09:18:14 AM »
Hello,

I think the only thing you can do is to find a servo valve with a CAN interface.

KR,
FStelzer

Offline slewis

  • PLUS+1 Developer
  • ***
  • Posts: 10
  • Karma: +0/-0
Re: Servo Valve requiring +/- 15v
« Reply #2 on: December 15, 2017, 04:20:53 PM »
Or, you could try using the Hbridge Output (eg: MC050-110, C1-P42 & C1-P43, OutputMode = 8 ).  I've used it to drive +/-10Vdc, so it should work for +/-15Vdc.

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +2/-0
    • Trebro Turf Equipment
Re: Servo Valve requiring +/- 15v
« Reply #3 on: December 15, 2017, 05:19:45 PM »
Thank you for the replies!