Author Topic: WARNING! Service Tool 2022.3.7  (Read 3480 times)

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
WARNING! Service Tool 2022.3.7
« on: November 16, 2022, 07:43:06 PM »
Hi, I just downloaded the latest ServiceTool and it has a serious and dangerous bug when importing parameter files, see attached pictures for an example.

The parameters "Transport_Page1_Enable" and "Transport_Page10_Enable" are Booleans but when I import the parameters into the parameter list in the latest ServiceTool it looks like the values from "Transport_Hinge_Flow_A" and "Transport_Hinge_Flow_B" is used instead of the actual values in the XML file.  :o

Same happens with other parameters in the list as well.
« Last Edit: November 16, 2022, 08:56:32 PM by Fredrick »

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: WARNING! Service Tool 2022.3.7
« Reply #1 on: November 17, 2022, 08:04:37 AM »
Hello,

I talked to the PLUS+1 Service Tool developers and found out that you are correct. There is an issue with importing XML files.
As far as I understood, the problem occurs when there is a difference between the XML list you import and the parameter list in the Service Tool. I don't have any more details.

My recommendation is to use the 2022.2 version until this is fixed.

Sorry about any inconvenience.

Best regards,
Tor
PLUS+1® SW PAE Team

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: WARNING! Service Tool 2022.3.7
« Reply #2 on: November 29, 2022, 07:23:16 AM »
Hello,

There's a new version of the PLUS+1 Service Tool, v2022.3.8, released in the Update Center.

Image from the release notes.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Re: WARNING! Service Tool 2022.3.7
« Reply #3 on: December 12, 2022, 08:51:10 PM »
Thanks, now it works well.
The new ServiceTool also appears faster then 2022.2, specially when it comes to downloading parameters.