PLUS+1 User Forum

PLUS+1 Hardware => Controllers => Topic started by: macbahi on March 08, 2022, 11:41:29 PM

Title: ExecTimeWork ?????
Post by: macbahi on March 08, 2022, 11:41:29 PM
Hi!

I use DM430E I use check point to see ExecTime,  ExecTimeGraph and ExecTimeWork but this last I can see it.
Please could you tell if ExecTimeWork is watching.  If yes Please show me how can I see it.

thanks in advance
Cordially
mac Bahi
Title: Re: ExecTimeWork ?????
Post by: Tor on March 09, 2022, 07:02:23 AM
Hello mac Bahi,

See attached image, it explains it a little better than I can.
This is taken from the DM1000 API specification, but I believe it works the same for the DM430E.
If you want even more information you can open the DM1x00 API from the hardware tab in PLUS+1 GUIDE (If you have the DM1x00 install that is), and search for "Main and Background Tasks".  There are some very useful information.

I hope it helps.