Author Topic: Display Scalable Image Library 70112442v100 is missing some svg files  (Read 2474 times)

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +6/-1
Hi,

I don't know if it is wanted or not, but a few symbols are missing in SVG format in the "Symbol" folder in the "Display Scalable Image Library 70112442v100" library.

I noted that at least these are missing when compared to the "000_Icon Chart.jpg" file :

- Fuel Level
- Engine Oil Pressure
- Lock
- Unlock

It would be nice if we could have access (in SVG format) to all the symbols shown in the "000_Icon Chart.jpg" file.

Addind to that, with the Tier4 / StageV requirements, I think it would be nice if you could add all the need DPF/Aftertreatment related symbols that are mandatory to be shown in a display screen. I know I can find them in the EIC program, but having these in SVG format would be easier.

Have a good day!

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 245
  • Karma: +25/-1
Re: Display Scalable Image Library 70112442v100 is missing some svg files
« Reply #1 on: April 30, 2020, 11:41:04 AM »
Hi,

Thanks for the information.

This library was created back in 2013 for the DP7XX displays, and I have my doubt this is updated after the EIC for the DP430 was released.
I will talk to the responsible people about this. Either they need to updated the library or maybe remove it.


Have a nice day, and stay safe.

Best regards,
Tor
PLUS+1® SW PAE Team