41
Displays / Draw lines and points
« Last post by F.M.Elettromeccanica on October 21, 2023, 07:41:34 PM »Hi all, i was wondering if there is a fast and easy way to draw lines and points dinamically. I have an array that defines a number of points (0 to 4096) and i wish to draw as points as the array length is. I can do this easily in other developement platforms (java,codesys,QT etc) but seems that is not possible to do it in GUIDE. i should to populate all 4096 elements in screen editor and them manage them manually???
. It' a huge work to do something that i can do in fwe lines of code in other dev envitonment. I hope i'm wrong...