Author Topic: HMR LED COLOR  (Read 2227 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
HMR LED COLOR
« on: April 11, 2023, 10:12:44 PM »
Hi guys,

Does anyone have experienced this issue with a HMR?

Basically I configured the LED´s for the soft buttons as blue, so everything did work fine for the 1st production

then a second production came up, all what we have to do is flash the controller, get everything connected and should be ready to go but guess what, now the HMR led color is yellow instead of Blue, I switch HMR´s between prod one and prod 2, and the one for 1st production does  light up blue no matter what production it is installed at, 1 or 2.

the problerm is that the one with the LED´s in yellow is always like that it does not get configured, just do not understand why

do you know what can be done or tested to understand and fix that?  the HMR block does not shows any error

thanks