Author Topic: Error 270 Invalid data in file  (Read 4783 times)

Martin s.

  • Guest
Error 270 Invalid data in file
« on: October 09, 2014, 10:53:31 AM »
 >:( >:( Any body knows what this error means, and how to solve it? I am getting when i try to download my project to a MC050-10

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: Error 270 Invalid data in file
« Reply #1 on: October 09, 2014, 12:03:12 PM »
I had this error one time also.
Do you have a version of the program that does not show this error?
If so Check all changes made, and re-do them.

If not I would remove blocks until the error goes away, and try to pinpoint where the problem is.

Maybe there is a better way, but the informations you have given. That is what I would do.

Hope it helps.

Martin s.

  • Guest
Re: Error 270 Invalid data in file
« Reply #2 on: October 09, 2014, 12:40:45 PM »
Great input! It showed out to be related to a Can Tx block, not sure what was wrong, by redoing the block solved the problem. Thaks for the input!

Martin

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: Error 270 Invalid data in file
« Reply #3 on: October 10, 2014, 04:59:17 PM »
Smells like something OS related, where maybe a newer CAN block, once compiled, is not compatible with older firmware/OS in an MC050-010.  What was the OS version?