Author Topic: BUG: Compilation aborted with error(s).  (Read 6295 times)

ET

  • Guest
BUG: Compilation aborted with error(s).
« on: September 21, 2012, 12:26:46 AM »
Sometimes, when I compile an existing program, the compiler window stops with "Compilation aborted with error(s)., but when I press OK, the error message box at the bottom of GUIDE is completely empty.
If I compile the program a second time, it works without any problems.

This usually only happens when I compile an existing program for the first time after re-opening it.
It happens with programs for MC50s, DP200s, and DP600s.

Quax76

  • Guest
Re: BUG: Compilation aborted with error(s).
« Reply #1 on: September 21, 2012, 08:00:09 AM »
I knew this problem, too. There is no error listed in the compiling window. This is pretty unfine...
This phenomenon also occurs. when I add an image to an excisting project an the name of the file contains 2 spaces in a row.

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: BUG: Compilation aborted with error(s).
« Reply #2 on: September 21, 2012, 09:16:17 AM »
If the lhx readme file is open, it also stops the compilation with a blank error window.
But in that case it does write the cause of error in the build window.