Author Topic: No IO Modules in Hardware List  (Read 922 times)

Offline STGBruce

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
No IO Modules in Hardware List
« on: January 17, 2025, 02:21:16 AM »
Thinking of using an IOX module on an application to add additional IO, but there are no IO modules in my hardware list.
I have tried going through update center, but don't see it in the available downloads.
Also tried searching online with no luck.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 301
  • Karma: +28/-1
Re: No IO Modules in Hardware List
« Reply #1 on: January 17, 2025, 07:14:54 AM »
Hello STGBruce,

If you don't see in the the Hardware tab it might be that you don't have installed the components from the PLUS+1 Update Center, and you have the PLUS+1 GUIDE setting to not show folders that are empty.
The setting can be found here: PLUS+1 GUIDE > Setup > Options > Tabs.  In the "Tabs Settings" you can uncheck the box "Hardware tab hides empty folders".

In PLUS+1 Update Center you have to select the components in your subscription, download and install them.
Click the "Edit" button in the top right corner, go to Content > Compliance Blocks > IO Modules.  Save selection, button on bottom right. Refresh (F5) if needed and install.

I hope this works out.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline STGBruce

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: No IO Modules in Hardware List
« Reply #2 on: January 17, 2025, 06:06:47 PM »
That was the help I needed, Thank you!