I've run into a problem with the MC088-015 controller while using the application log. My program compiles with no errors, but I lose communication with the controller once I download it. If I remove the application logging features from the program and recompile/download everything is fine. The only parts of the program I remove to make it work again are the "Define Application Log Areas Page", the "Define Application Log Page", and the "Access App Log Enable" component. I'm using the latest hardware file (10108098v170), but I have also tried with an older version (10108098v150).
Has anybody seen this before, and know what's wrong?