PLUS+1 User Forum

PLUS+1 Hardware => Controllers => Topic started by: MimmoA on November 13, 2013, 03:19:39 PM

Title: Pin output configuration
Post by: MimmoA on November 13, 2013, 03:19:39 PM
Hello,
I need to use the joystick input to have an output in mA .
I scaled the Xaxispsn  (-10000/+10000) with the range i need for output 200/560 mA.

Which pin do you advice me for this situaion?Is there a difference?
And how do I have to set "Outputvalue"  and "pinconfig" in the  pin?

Thank you so much in advanced,
Mimmo.
Title: Re: Pin output configuration
Post by: MimmoA on November 13, 2013, 03:58:57 PM
Solved..... ;D ;D
I setted Ouputconfig with a "4" value.
Thank you