PLUS+1 Hardware > Controllers
Using MC024 to control s20 pump
(1/1)
Mr.Jacobee:
Hello,
Could anyone tell me if it is at all possible to use PLUS+1 software to control pumps like those from s20? Better yet, is there any way to change output current on a pin ? Let's say I use standard s90 EDC block in GUIDE and I want to get it to 100mA (while standart for EDC on s90 should be 85mA)?
Thank you all in advance.
FluidPowerTom:
You can control current as high as you like up to 3,000 mA on most outputs. I'm not sure if you'd do this by changing a setting in the S90 compliance block or by just making your own code, but either way I think it'll work fine.
Lukey:
If using the S90 EDC block then yes you can change the max current to 100mA, changes are made in the Config_data page of the compliance block.
Mr.Jacobee:
Thank you guys very much ;)
Navigation
[0] Message Index
Go to full version