General Discussion > Functional Safety and PLUS+1
Checking primary and secondary cores are functioning on SC050
(1/1)
jashom1:
Hi,
Due to the outcomes of a risk assesment, we have determined that we need to check to see if the primary or the secondary core are responding and functional. My question is do I need to go as far as exchanging an RS232 message between the cores, or can I just do a simple check with the SafetyLayer bus on the signal "Failure" to determine if it's zero or not, then disable outputs based on that?
Has anyone done any examples?
Thanks!
John.
Navigation
[0] Message Index
Go to full version