PLUS+1 Tools > PLUS+1 GUIDE
Service Tool Data in Guide
sanjeewa:
@acmall, I was looking a way to set those data section inside the program. So that I can change it in the program and compile. Won't need to update at multiple places as version is specified in the program.
Lukey:
You want to use Non-volatile Memory Dynamic or Non-voilatile Memory Dynamic Input blocks
This will allow you to access from the service tool and adjust, the NV Memory will retain this information on power cycle.
acmall:
Hi @sanjeewa
The screen shot I posted is inside the program. The info entered there can be viewed in the service tool using string parameter components: -
#ECUInfo.ApplicationId (This is Description, also shows beside the node in the ECU list)
#ECUInfo.SystesmId
#ECUInfo.ApplicationVersion
#ECUInfo.ApplicationType
Note that it you enter a value for Type you will get a warning when downloading the program if the existing program type does not match the new program type. You have to enter the new valve for type to confirm.
Navigation
[0] Message Index
[*] Previous page
Go to full version