Author Topic: PLUS+1 GUIDE and Service Tool 2022.1 is released  (Read 5311 times)

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
PLUS+1 GUIDE and Service Tool 2022.1 is released
« on: April 22, 2022, 10:10:52 AM »
Hello,

You can now download and install the latest version of PLUS+1 GUIDE and Service Tool from the PLUS+1 Update Center:  https://youtu.be/4n8f8ri-poY


Information from the Release Notes:


PLUS+1 GUIDE
New Features and Functionality (see the GUIDE User Manual for more detailed information)

[F00607] Feature: Install LHX for Linux in PLUS+1 Service Tool
- It is now possible to install diagnostic data from an LHX file of a Linux-based HWD in PLUS+1 Service Tool.

[F00528] Feature extension: Static Analyzer Improvements
- It is now possible to use over 40 different metrics.
- It is now possible to import/export Static Analyzer settings.
- It is now possible to configure a limit for how many warnings should be shown for each warning type.
- It is now possible to run the Static Analyzer in command line mode.
- It is now possible to use “Suppress Warning Start” and “Suppress Warning End” components to disable a specific Static Analyzer warning within a code area. - The coding guidelines document has been updated and is accessible in the “Help” menu (P100003179).

[F00617] Feature extension: New nodes have been added in the hardware tree for Programmable Valves, Electrical Converters, and PLUS+1 Partner Products. (W01418)

[W01158] Feature extension: A dialog is now shown when closing the License Manager when the license needs activation or rehosting.



PLUS+1 Service Tool
New Features and Functionality (see the Service Tool User & Design Manuals for more detailed information)

[F00555] Feature: Signal Logger (requires HWD support)
- Select up to 10 signals to log where sampling period, duration and optional trigger events can be configured.
- Logged signals are displayed in a configurable linear diagram with zoom functionality.
- Load/save configurations (in XML format).
- Load/save logged data (in CSV format).
- Optional auto save functionality for logged data.

[F00532] Feature extension: Float data types support in Advanced Pages
- 32-bit and 64-bit float type signals are now supported in Advanced Page components.
- Only available for protocols where these data types are available.

[W01158] Feature extension: A dialog is now shown when closing the License Manager when the license needs activation or rehosting.



Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: PLUS+1 GUIDE and Service Tool 2022.1 is released
« Reply #1 on: April 22, 2022, 05:24:08 PM »
Thanks for the update Tor.  I'd like to request an instruction video for the Signal Logger get added to your Youtube page.  You mention HWD support... will most MC controllers support this?
Controls Engineer
Hydra-Power Systems

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Re: PLUS+1 GUIDE and Service Tool 2022.1 is released
« Reply #2 on: April 27, 2022, 09:02:29 AM »
It looks like this release mostly concentrated on bug fixes, not much in the way of new functionality. Not necessarily a bad thing but I have been hoping that the functionality for displays will be enhanced.

It appears that there is currently very little HWD support for the signal logger. I have tired MC088, MC050, MC038, SC050, DP610TM, DP720 & DP570 and none of these appear to support the signal logger with the most current HWD versions available in the Update Centre.

Will there be updates to the HWD files to support this? Which units do currently support it?


Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: PLUS+1 GUIDE and Service Tool 2022.1 is released
« Reply #3 on: April 27, 2022, 04:22:06 PM »
Hello,

Yes, I believe the signal logger is only supported by some versions of the XL controller.  I'm waiting for response from the developers about what the plans are for the future.
The signal logger video is in the video list, it just need to be made.  ;)


Hang in there.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: PLUS+1 GUIDE and Service Tool 2022.1 is released
« Reply #4 on: May 04, 2022, 10:54:10 AM »
Hello,

As of now only new products will support this function, like the XL104.
If there would be high demand for SC, MC and DM devices this needs to get pushed by product management. So let your Danfoss sales person know if there is a demand for this.

Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team