PLUS+1 Tools > PLUS+1 GUIDE
Project .p1x not found in folder
Tor:
Hello,
Some updates regarding this issue. It looks like it's a change in some web browsers (using Chromium).
If you are using Firefox there is a way to get all the links "fixed". You can open the html file directly in Firefox.
Where to find the html file.
Displays using build folders:
- Open the build folder (there is a link in the Error/Warning/Hints tab for the Build path).
- Locate the html file.
- Right click and open with Firefox.
Other units:
- Open the project folder (File -> Open Project Location)
- Locate the html file.
- Right click and open with Firefox.
The links in the browser window should take you to the error location in PLUS+1 GUIDE.
If you are using other browsers.
- Copy error link (right click and "copy link")
- Paste in browser
- Add slash and colon if it's missing ("plus+1://C/project" -> should be -> "plus+1:///C:/project")
- Press enter and you should see the location of the error in PLUS+1 GUIDE.
Lukey:
Hi Tor I followed your instructions but once I open the link in my browser (Chrome or Edge) I get taken back to GUIDE and received the same message about .p1x being missing, it is an infinite loop, I cannot see where the error is.
Tor:
Hi Lukey,
You have to make sure the path is correct, one slash and a colon is missing when it shows up in GUIDE.
After some changes in Chromium, used by several web browsers, to make it more secure, it doesn't take the path provided by GUIDE.
This is how I do it to make sure all is good.
- Compile.
- Open the project folder (File -> Open Project Location)
- Locate the html file.
- Open in a browser.
- Copy the Error link into note pad or similar program.
- It looks like this:
plus+1://C/Projekt/PAE/HW_Projects/SC050_020_Prim/SC050_020_Prim?page=SC050-120-122-PRIMARYT!TOP!Application;x=2750000;y=725000;ind=Error
- Edit the link by adding a slash and a colon to it.
plus+1:///C:/Projekt/PAE/HW_Projects/SC050_020_Prim/SC050_020_Prim?page=SC050-120-122-PRIMARYT!TOP!Application;x=2750000;y=725000;ind=Error
Note the added slash and colon "plus+1:///C:/Project...."
- Copy the edited link and Paste it to Edge and press enter.
This works for me.
A fix is on the way.
Lukey:
Ah yes my bad, that works, thank you.
Tor:
Hello all,
The new version with the fix for this problem is uploaded to the PLUS+1 Update Center, version 2024.3.5.
To download/see this version you need to update the Update Center as well.
Have a nice day.
Navigation
[0] Message Index
[#] Next page
[*] Previous page
Go to full version