PLUS+1 Tools > PLUS+1 GUIDE

Compile Warning 39

(1/1)

dlewis:
I'm starting to work with a safety controller SC024-110 and when I compile the program I get the following messages.

Graphic Compiler has created warnings, continue anyway?

*** WARNING 39 *** [GLINK] SYS: No exact match (SYS/SYSI) found for HW signal: {CAN[0].Baudrate} with Reftype: {SYSI}. This will be an error in future version of GUIDE.

Tor:
Hello dlewis,

The "Warning 39" is a OS bug that has been changed into a warning so it is possible to compile the project.
This Error are in certain HWDs and they are working on a solution.

We have found a workaround to "remove" it, buy moving the "Inputs" block before the "Unit_Config block". Then the error should go away. (In the image is a SC050, that's what I had open in GUIDE).


Have a nice day.

dlewis:
Thanks. Moving the input block took care of the warning.

Navigation

[0] Message Index

Go to full version