Author Topic: Toggle between Screen Area Pages  (Read 7382 times)

bgtwuk

  • Guest
Toggle between Screen Area Pages
« on: November 14, 2010, 02:29:14 PM »


Good Morning

I am new at this of course. I have two screen area pages, and am trying to select between them with a soft button.

I have an enable port for each page, that I believe should have the proper affect.

Am using a simple switch but my pages are not toggling properly.

The fog is thick up here eh!

Bgtwuk

Thomas

  • Guest
Re: Toggle between Screen Area Pages
« Reply #1 on: November 15, 2010, 11:54:27 AM »
Hi!

Have you connected your enabling signal inside the Area? It is very easy to forget.




Best regards // Thomas

bgtwuk

  • Guest
Re: Toggle between Screen Area Pages
« Reply #2 on: November 15, 2010, 12:14:12 PM »


Very Interesting.

I will try that.

Thanx


Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Toggle between Screen Area Pages
« Reply #3 on: October 15, 2013, 05:56:23 PM »
Hi,
I have another question about toggling area pages:

I have a program with very much area pages.
Now, I have to add a new area page which can be placed everytime and everywhere on display.
It is a "help-screen".

My question:
Is it OK to switch on this new area page and it will appear in front of all other areas?
If I switch off this help-menue it will disappear and the screen is as it was before this action.

Is there a rule like: The last area wins?


Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Toggle between Screen Area Pages
« Reply #4 on: October 18, 2013, 11:08:53 AM »
Hi Bernd

Yes that is correct.
And the last area of the enabled areas wins.


Best regards
Daniel
PLUS+1® HelpDesk
PLUS+1® Help Desk Team

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Toggle between Screen Area Pages
« Reply #5 on: October 18, 2013, 11:53:21 AM »
Thanks,
but one question about Thomas' two linked area pages from NOv. 15 2010:

Does it work if they are linked?
If I copy an area page and don't delete the linking of them, the compiler produces an error.

Is it possible to copy area pages and link them?
I think, there would be a problem, if you want to assign a screen page to one of them, because they have the same name.....
I'm working now with Guide 5.0.8 .
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung