PLUS+1 Software > Displays

Communication between DP210 and microcontroller MC24-XXX

(1/3) > >>

fhm1963:
I need to know how communicate a display DP210 and a micro MC24-XXX. Can anyone tell me where I could find info of it?

Jakob:
If you use the standard CAN-tx and CAN-rx function blocks, you will be well on your way.
Just remember, all CAN-messages are type U8, and you will have to convert and check if your signals valid.

Jakob:
?

Maxim:
Hello,

This is an old topic but it is just what I need.

I have almost the same setup and I need to do exactly the same but I can't get this to work. Would it be possible to help me out on the connections that have to be made on the block?
The goal of the setup is to use the soft keys on the display to control the program in the controller.

This is the correct block?


I'm sorry but I have very little knowledge of this software, I was thrown in this due to illness of a colleague.

Thanks in advance.

Jakob:
Yes that is the right component for receiving a CAN message.
The RX function should be in the controller program.

Have you looked at the help file for this component, there are usually some helpful examples there.

Navigation

[0] Message Index

[#] Next page

Go to full version