PLUS+1 Software > Communication
Sauer-Danfoss CG150 cable and codesys
(1/1)
ripplingwater:
hi,
I have a Sauer-Danfoss CG150 CAN to USB cable ( image attached ) and I was trying to connect an Connector Interface Board ( connected to an ECU ) to CODESYS 2.3. The earlier cable used was a PEAK CAN Cable that I am not really sure of but then I was wondering the comm settings when using Sauer-Danfoss CG150 cable. The rest of the settings are default ECU comm settings and should be fine but there is one field called "CAN card driver". I was wondering what is the value to use for that? I have attached a screenshot. Many thanks
Screenshot:https://imgur.com/a/nmzmQ
Cheers,
RW
Navigation
[0] Message Index
Go to full version