PLUS+1 Software > Code sharing
Temperature Sensor
(1/1)
thatoneguy:
Hello out there,
Really green on Plus 1 programming.. had a question on Temperature Sensors does anyone have any examples on how they need to be implemented? I plan on using the standard Liquid Temperature Sensor...Any help/examples/point in the right direction would be awesome!!
Thanks
spittet:
There is a function block that already has the required "ohm vs temp" function built-in. This block is located under the Hardware Tab : Sensor-StandAlone/Temperature/Liquid Temperature Sensor/SubTemplate.
Simply feed it the input pin and it will retrieve the ohm value from it. Then, it will output the temperature, either in °C or °F, as you wish.
Sam
thatoneguy:
Thanks Sam.. I got that figured out I thought there was more to it than just hooking it up to the Ohms.
oiltronic:
Just be aware of the ohm limits on the input pin you wish to use. because some will clip at 10k, which I think is around -5C. But if your oil is that cold there are probably other issues...
Navigation
[0] Message Index
Go to full version