PLUS+1 Hardware > Controllers

MC050-020 Troubleshooting

(1/1)

CShultz:
Hello,

I have a problem connecting the MC050-020 with my CG150..
I have measured 60ohms resistance on my connection.. I measure 2v when I ground C1p3 (CAN0+) and the same when I ground C1p4 (CAN0-)
... Also checked C1p20 (CAN1+) I get 0v.. But I do get 2v when I ground C1p21 (CAN1-).
I have successfully hooked up my MC024-010 as well as a DP200.. so I know things are working the way they are supposed to.
Is it possible I fried the MC050-020?
Anything else I can try?

CShultz:
Problem Solved.  Help Desk was great at getting back to me so quickly.
It was a simple Baud Rate mis-step.  Rookie move, goofin around.

Navigation

[0] Message Index

Go to full version