PLUS+ Tools > PLUS+1 GUIDE CANKing

CAN-king doesn't start-up

(1/1)

Lammert:
Hello,

I try to start-up CAN-king for the first time and get the message: Exception EOleSysError in module wc32.exe at 000AD6E5. Error while access to the OLE-register.

I use a new Asus laptop i3 Core with Windows 7.

I try to install CAN-king again but get the same application error.

Is there anyone who can help me.

Thanks in advance.

Lammert

Andy:
Right click the shortcut and select "Run as administrator". That should do it.

Lammert:
Thanks a lot, it works.

Stefan:
Hello,

To get it to run as an administrator every time, do like this:

Right click on the icon and select Properties.
Click on the tab Compatibility and check Run this program as an administrator.

With this setting you can start the program the usual way.

Best regards
Stefan

pinias:
Hey There,

This infor also helped to me

Thanks

Navigation

[0] Message Index

Go to full version