PLUS+ Tools > PLUS+1 GUIDE
Search/Replace Signal Names [Resolved]
PatrickS:
I'm working on updating a program and have decided that some of our old signal names should be changed to be more descriptive.
I've found the Search/Replace dialog within Plus +1 and the Search functionality works fine. However; I cannot get the Replace functionality to work at all. To me it looks like that the main issue is all replaceable item checkboxes are greyed out, so when i go to update the replacement list I just get the message 'There are no items to replace checked'.
Am I missing a setting somewhere or is this functionality just not available?
acmall:
If I remember correctly the Replace functionality is only available for the Vector Based Screen Editor.
Tor:
Hi PatrickS,
I'm sorry to say that the Search & Replace function only works for items in the Screen Editor for now. So if you open a display application the boxes won't be grayed out.
I believe it's because of some limitation within the CAD engine that is used for GUIDE, and as far as I know the developers are working on it.
This is something that could/should be stated in the manual.
Have a nice day
(Edit: acmall was quicker than me.)
PatrickS:
Oh ok, thanks, I tried looking through the manual but either didn't see that limitation or didn't understand it.
Anyway thanks for your help, when i get to updating the display, i see if Replace works then.
Tor:
Hi PatrickS
I was a little bit unclear in my post.
I can't find it in the manual either, but it is something that should be stated in there. I will point this out to the responsible people.
Thanks for letting us know.
Have a nice day
Navigation
[0] Message Index
[#] Next page
Go to full version