PLUS+1 Tools > PLUS+1 GUIDE
Transmit CAN with Encode 8
FluidPowerTom:
--- Quote from: Mike on December 08, 2020, 06:22:01 PM ---With that particular block it should be included inside the block. The description states:
" Send (Bool):
False to true transition will send the PDO.
T: Positive transition will send the PDO
F: Do not send PDO"
But yes I believe if using the basic CAN blocks that you would have to add that transition element yourself.
--- End quote ---
Sounds like they may have built it into that compliance block then based on that description.
Navigation
[0] Message Index
[*] Previous page
Go to full version