PLUS+1 Hardware > Displays
Service tool and DM1200T
Mike AA:
So I have started programming my DM1200 and went to upload the first program I wish to run. When I started the transfer with my CG-150 I let it sit for over 30 minutes and it was maybe 15% done. I disconnected and restarted with my CG-150-2 figuring maybe it would be a faster transfer speed. 10 minutes in and its maybe at 20%. Is this indeed this slow of an upload due to everything going on with the DM1200 or am I just seeing something odd going on? This is the first upload I am making for it.
Thanks,
Mike
Beezkneez:
When I was playing around with the DM1000 I saw the same. If you look at the size of the LHX file compiled for a DM1000/DM1200 you will notice they are significantly larger than an LHX compiled for a DP6xx or DP7xx. I found that if you wait long enough the CG-150 will do the job, but I highly recommend ditching the CG-150 and using the USB interlink gateway. Downloads to the DM1x00 display using the interlink gateway take about 8-20 seconds.
pinias:
Hey Guys,
ok, the 1st time you flash the DM display takes around 3 to 4 hours if you use the CG150, I think it configures everything.
next time you flash it, it will be around a minute with the CG150.
by the way, make sure you are using the latest HWD version, the previous version had an issue with the NV memory, basically it did not retain the value after cycling power.
as far as I know from the PLus1 help, the latest HWD version fix that
Mike AA:
The long time is indeed only the first upload. I just changed the layout and reloaded in 30 seconds. Its missing a bunch of graphics and more stuff but way better than the over 2 hours for the first upload.
How do I use the USB interface? I had two from wanting to try on the DP720 but never got it to work right. I'm guessing I am missing drivers.
Mike
Stefan:
Hi,
You need a special cable for DM1000 and DM1200. You can order it from your Danfoss distributor and the part number is 11231512.
Best regards
Stefan, PLUS+1 Helpdesk
Navigation
[0] Message Index
[#] Next page
Go to full version