PLUS+1 Hardware > Controllers
SC024 Output problem
G30RG3:
Maybe the controller takes a false ground over the CAN network, but if you break the ground wire, I would expect the controller to malfunction in a random way.
I'm glad the controller survives this at all. Missing one of the 3 12 volt wires is bad if the current draw is too high on the remaining pins, but sinking a current over whatever is left doesn't seem healthy.
macbahi:
Hello Guys,
I have good news for you
I was tested again my controller in order to be sure when disconnect wire ground all output off controllers turns ON even though the Outputdisabled = 1 (secondary). It's not normal. You will find included the test sent to Plus +1 help.
To be brief, I suggested to Sir Randy to make a test in order to convince him. Finally Randy did it and he was convinced.
Here is his answer.
As I told in the my first message of this topics I was sure the problem.
I hope this case will help you
With best regards
Hamid
Navigation
[0] Message Index
[*] Previous page
Go to full version