PLUS+1 Hardware > Controllers

SC024 problem Can

<< < (2/2)

Camox:
Hello,
We had a case where a module overloaded the CAN and made all the modules invisible when it was plugged in.

Have a nice day!

macbahi:
Hello guys,

Thank you very much guys to answer me.

acmall: Yes I tried to do Recover ECU but without any result.  Service tools message:  No ECU found.

G3ORG3: the baudrate in module was 250K  and now I connect with service tolls using baudrate 250K.

camox: overloaded CAN. As I told you sir in my last message I only connected one module at a time.  So I don't know overloaded CAN in my case.
                                      When I use the other module at service tools icon Busload shows 8%.

Unfortunately, so far I have not been able to resolve this issue.

Thank you very much

With best regards



G30RG3:
My suggestion is to use a scope to check the signal with only the suspect and a termination resistor. 
Since you said earlier that the scanning becomes impossible, the device at least disturbs the CAN signals, so you should see something, good or bad, timings, deformations, ...

Navigation

[0] Message Index

[*] Previous page

Go to full version