Author Topic: 5 Volt DOUT  (Read 3833 times)

Offline F.M.Elettromeccanica

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +1/-0
5 Volt DOUT
« on: October 10, 2020, 04:13:57 PM »
Hallo gurus,
Is there a way to have a 5v DOUT DC on a MC050-110? I wish to avoid to install a DC/DC Converter...
Thanks in advance

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: 5 Volt DOUT
« Reply #1 on: October 12, 2020, 12:50:20 PM »
Hi,
there is sensor power pin on c1p8 and sensor power ground on c1p9.
You can't switch it.
I believe, max current is 360mA.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: 5 Volt DOUT
« Reply #2 on: October 12, 2020, 07:05:30 PM »
If you did need a switchable 5 VDC out you'd have to use an output set to Duty Cycle control and reference the supply power along with a little math to make the duty cycle create a 5V output.  In my experience you can keep it within 0.05 volts or even better accuracy.  That said it's certainly not going to be a true regulated 5 V out like on pin 8.
Controls Engineer
Hydra-Power Systems

Offline F.M.Elettromeccanica

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +1/-0
Re: 5 Volt DOUT
« Reply #3 on: October 13, 2020, 08:47:07 AM »
Thanks everyone for the answers.  In fact it is exactly what I did, only it seems that the problem is the frequency (max 4khz).  I believe I will take a PWM / DAC converter to have an effective DC current

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: 5 Volt DOUT
« Reply #4 on: October 13, 2020, 11:23:06 AM »
And please think about, that hardware couldn't output more than 5V, if there would be an software error!

Do you need a switchable 5V supply or do you need a voltage output between 0 and 5 V regulated? And what current?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline F.M.Elettromeccanica

  • PLUS+1 Developer
  • ***
  • Posts: 47
  • Karma: +1/-0
Re: 5 Volt DOUT
« Reply #5 on: October 13, 2020, 04:03:08 PM »
Hi Marbek, I need a voltage regulation between 0 and 5V
500mA max

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: 5 Volt DOUT
« Reply #6 on: October 14, 2020, 09:16:30 PM »
How many pieces every year?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung