70
« Last post by a.damato on February 16, 2024, 09:24:05 AM »
Hello Everybody,
I would like to ask some question regarding the block "Read Array from Application log".
When i try to read the "LineCount" Output. I get a weird amount of line.
I am using a DM1000, menu buttons , no Touch.
In the help manual i read X6 : Total number of lines in the application data log.
So i should get from this output 1,2... depending on the amount of line in the applog file.
Right now i am using a trick that register the number when i switch on the Display.
Because it's reading right when i switch on the device but in the moment i write a new line this number has a weird behaviour.
I am wondering if anyone had this issue?
Thanks.