PLUS+1 User Forum

PLUS+1 Software => Displays => Topic started by: BBarry on August 29, 2022, 03:53:02 PM

Title: Max size for a text list?
Post by: BBarry on August 29, 2022, 03:53:02 PM
Hey Brilliant People!
Looking in the manuals I could not find this. For the DM430.

Is there a size limit on the Text Lists? (outside of the u8 0-255) limit on the Active Index?

Like total string char limit?

I am planning to use a text list for alarm history page and need to know if I am limited to the number of alarms (text strings) I may have in a list?

Warmest regards,
Title: Re: Max size for a text list?
Post by: Tor on August 30, 2022, 11:18:40 AM
Hello BBarry,

As far as I could find after asking the PLUS+1 Team there are no direct limitations for the text list.
The type of the signal, memory and how much time you have to add alarm texts.
And I believe that the Active Index is not limited to a U8.

I hope it helped
Title: Re: Max size for a text list?
Post by: BBarry on August 30, 2022, 04:07:36 PM
That did help. Thank You!