Author Topic: Target OS does not match file OS.  (Read 4481 times)

ET

  • Guest
Target OS does not match file OS.
« on: June 21, 2012, 10:56:00 PM »
Trying to upload new software into a DP600 I'm reprogramming.
After hitting the last download button, I get the error:
Code: [Select]
Target OS 10103292v160 does not match File OS 1010329v180Is it safe to ignore this and proceed with the download, or should I upgrade the OS on the display?
If I need to upgrade it, what are the necessary steps?

Offline mebib

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +0/-0
Re: Target OS does not match file OS.
« Reply #1 on: June 21, 2012, 11:47:51 PM »
This is not an error message, just a warning.
The message is telling you that you are on the way to update the OS to the new version 180 (newer version of the .hwd file). You can ignore the message and continue with the download. No further action is needed.