Recent Posts

Pages: 1 2 [3] 4 5 ... 10
21
PLUS+1 Service Tool / Re: Image repository directory not found.
« Last post by Fredrick on September 06, 2022, 10:57:07 AM »
Anyone else having problems with this?
Also, sometimes the P1D file does´t get saved so next time you open the P1D file the changes are lost and you now have an older P1D file without the changes you just did. :(
22
Displays / PIB - DM1x00 HWD file update
« Last post by Tor on September 02, 2022, 10:07:18 AM »
Hello,

If you have not seen the latest PIB (Product Information Bulletin) about the DM1x00 I would like to share it here.

In short:
An issue was found that can cause the device to lock and become unrecoverable. The advice is to recompile to .HWD v308 or greater for any devices with a manufacturing date of August 11 or after.
The HWDs are located in the PLUS+1 Update Center. The version stated in the Update Center is 3.8.0 for some reason, but it's v308 when installed in GUIDE.

More information in the attached image/PDF file.


Thank you.
23
Code sharing / Re: PGN 65259 SPN 588
« Last post by Matt_Eng on September 01, 2022, 08:20:10 PM »
I agree the result does seem a little strange. However, it should be possible to convert the ascii array to a string to make it easier to read.
Should just be a Retype to String, and then the checkpoint can be read in the service tool with a "String Parameter" in an advanced page.
24
Code sharing / Re: PGN 65259 SPN 588
« Last post by acmall on September 01, 2022, 09:09:41 AM »
I have not used it so you will need to confirm this but, I would have expected the CI_Parser to return an array of ASCII codes. What you are getting back doesn't appear to be a serial number when converted.

55 = 7
29 = [GROUP SEPERATOR]
41 = )

What make of engine are you getting the serial number from? In your code PGN 65259 is being requested from Node ID 3. Per J1939 ID 3 is normally Transmission #1, 0 is Engine #1 & 1 is Engine #2.
25
Code sharing / Re: PGN 65259 SPN 588
« Last post by macbahi on August 31, 2022, 09:51:42 PM »
Hi Acmall,

You are right, it's working now.
I get 2 data: motor serial number size and motor serial number

motor serial number size = 8
motor serial number[1]= 55;
motor serial number[2]= 29;
motor serial number[3]= 41;
......
motor serial number[8]= ;

Is't that  motor serial number 552941........

Thank you very much
with best regards
26
Code sharing / Re: PGN 65259 SPN 588
« Last post by acmall on August 31, 2022, 09:15:41 AM »
Is the Source and Destination mixed up for TP_RTS_CTS_Rx1?. I think Source should be the device you are receiving from and Destination is the Local address.
27
Displays / Re: Real Time Clock For DM430
« Last post by Tor on August 31, 2022, 07:17:46 AM »
Hello BBarry,

The Real Time Clock signals in the DM430 are located in the "TOP ! Inputs ! Time" page in the template.
You can also find them in the API Specification. It's located in the HWD folder, in the project manager in PLUS+1 GUIDE.
There's a YouTube video about the RTC for the DM1000, but it should work the same for the DM430.
https://youtu.be/6yGlqbo6TuM


I hope it helped.
28
Displays / Real Time Clock For DM430
« Last post by BBarry on August 30, 2022, 04:30:50 PM »
Hello again!
Is there a RTC on the DM430? I am assuming no since I see nothing about it on the message boards or manual. If so.. How do I access it?

The unit will be powered off and on regularly so creating a clock in the code will not work.

Thanks again for everyone's help.
29
Displays / Re: Max size for a text list?
« Last post by BBarry on August 30, 2022, 04:07:36 PM »
That did help. Thank You!
30
Code sharing / Re: PGN 65259 SPN 588
« Last post by macbahi on August 30, 2022, 02:43:02 PM »
Hi All,

I am using PGN 65259 in order to get motor serial number as you see in Matt_Eng example.

As result usually a serial number_size = -1;

Please could you tell me where is the problem

Thanks for your help

With best regards
Pages: 1 2 [3] 4 5 ... 10