PLUS+1 User Forum
PLUS+1 Hardware => I/O Modules => Topic started by: macbahi on October 25, 2023, 09:50:57 PM
-
Hello,
I usually use SC050 ou SC024 CAN0 with module OX024-110 Can0. It's work very well.
But now I am changing my communication with CAN1. So I can not see my module OX024 -110.
Please the CAN+ CAN- of module OX024-110 can be CAN0 and CAN1. Or only CAN0.
Thany your for your help
With best regards
-
I can't comment from personally experience but the first thing that comes to mind;
In your SC GUIDE program have you changed the CAN address for the Expansion Module to CAN 1 ? as default is CAN 0 I believe.
-
Thank you for your reply.
Finally it's correct but I don't know why In service tools the module OX024 is connect to CAN0 despite being connected to CAN1 in guide.
Please see image. And also I can not see the SC050 secondary.
But it's working.
Thank you for your help
With best regards
-
It's possibly because your CG150 is physically connected to CAN0?
-
The ECU list shows the port that you have connected to on each device. As the OX024-110 only has one CAN port this is showing as CAN 0.