PLUS+1 User Forum
PLUS+1 Hardware => I/O Modules => Topic started by: pinias on August 13, 2013, 04:08:01 PM
-
Hello There,
mmm I have a DP610, DP200, Controller MC050, Controller MC012-10 and a I/OX24-10 but It seems that I need a MC024 controller becuase of the room where it is going to be installed.
I think most of you have realized that the I/O modules look alike to a controller so I wonder to know if there is a way to convert a I/O module to a controller
for instance as I mentioned above, I have the I/OX24-10,
Could it be posible to convert it to a MC024-10 controller?
if posible it will be great.
Does anybody knows if that is posible?
if so, what is needed?
I appreciate your feedback
Antonio
-
Hello Antonio
I doubt that it is possible, not without some hardcore hacking of the unit anyway.
In which case I'm pretty sure that your warranty would be void.
Also the OX-module and MC differs very much on the inside.
The OX would not be able to perform the same tasks as a Controller.
But this is just my thoughts on this, it wouldn't surprise me if somebody has done something to an expansion module just for fun.
Regards Jakob