Author Topic: CS500 GUIDE Intergration / Function Block ?  (Read 3232 times)

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
CS500 GUIDE Intergration / Function Block ?
« on: October 26, 2023, 02:53:08 AM »
I am integrating a CS500 into an system with a DM1200 display as the main controller.

I'd like to pull GNSS information from the CS500 to the Display.

With the CS500 Service Tool I can send this info with CAN messages but then I have to decode them in GUIDE to show the on my Display, and I cannot see a way to get speed or heading to be sent.

Is there an easier way with a Function Block to do this? I cannot see anything in GUIDE or Update Center, am I blind or ignorant?

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 39
  • Karma: +3/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #1 on: November 10, 2023, 04:14:08 PM »
Hello Lukey,
You can send the GNSS position by setting the parameters of the CAN messages transmitted by the service tool :


I hope I've helped you.
I'm sending you the CS500 diagnostics file.

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #2 on: November 12, 2023, 10:32:54 PM »
Thank you Camox, unfortunately that function does not work.
After much trial with no luck and discussion with Danfoss through the help center I'm told that in the v114 update that feature was broken, I now await the release of the latest software so that GNSS data can be configured to be sent automatically  or with the Virtual Signals feature.

Offline mvanwiechen

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #3 on: November 16, 2023, 02:48:35 PM »
Thank you Camox, unfortunately that function does not work.
After much trial with no luck and discussion with Danfoss through the help center I'm told that in the v114 update that feature was broken, I now await the release of the latest software so that GNSS data can be configured to be sent automatically  or with the Virtual Signals feature.
I have the same issue.... periodic sending of the GNSS data onto the CANbus stopped working after updating firmware to v114.  Helpdesk has told me it will be fixed in v116 of the firmware.

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 39
  • Karma: +3/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #4 on: November 20, 2023, 08:37:57 AM »
I have the same issue.... periodic sending of the GNSS data onto the CANbus stopped working after updating firmware to v114.  Helpdesk has told me it will be fixed in v116 of the firmware.

Hello,
Thanks for this information.
We had a lot of trouble with version 114. I hope version 116 will be available and stable soon.
Have a good day

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #5 on: November 30, 2023, 03:15:11 AM »
I can confirm v115 release has not fixed the GNSS messaging over CAN via Virtual Signal Triggers or Periodically timers.

Fingers crossed for imminent v116 release fix.

Anyone know where an update/fix log for v115 firmware can be found/downloaded?

Offline Camox

  • PLUS+1 Developer
  • ***
  • Posts: 39
  • Karma: +3/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #6 on: December 01, 2023, 02:04:07 PM »
Quote
Anyone know where an update/fix log for v115 firmware can be found/downloaded?

I don't know if this information is provided by Danfoss.

Have you asked support?

Offline mvanwiechen

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #7 on: December 01, 2023, 04:20:20 PM »
I was wondering the same, regarding update log for a new version of the firmware.

I'm not sure if it is worth my time to update to v115, or if I should just wait to v116.

Offline Lukey

  • PLUS+1 Developer
  • ***
  • Posts: 49
  • Karma: +5/-0
Re: CS500 GUIDE Intergration / Function Block ?
« Reply #8 on: December 03, 2023, 04:38:30 AM »
Danfoss support was unable to provide a change log but have been very helpful otherwise.

Yes I recommend waiting till v116 if you're wanting to send GNSS data over the CAN bus.