Recent Posts

Pages: [1] 2 3 ... 10
1
PLUS+1 Compliant Hardware / Re: JS1H - Digi out
« Last post by magitec on March 29, 2023, 06:46:14 PM »
Perfect thank you. just a few other questions i'm using the PMW output for a 12v reversible output to control a 12v actuator forward is 0 - 12v and then backwards is 12 - 0v which PID file do i require for setting up the limits / proportional control scale.

again thank you, its not something i have used before, i do have the correct CG150-2 cable
2
PLUS+1 Compliant Hardware / Re: JS1H - Digi out
« Last post by FluidPowerTom on March 29, 2023, 06:09:16 PM »
It looks like it's a yes on all accounts
3
PLUS+1 Compliant Hardware / JS1H - Digi out
« Last post by magitec on March 29, 2023, 05:26:57 PM »
Hi,

I have a JS1H with 2 buttons, one on the top and one on the shaft (OP present) on the wiring pinout i have on the black connector a Dig out 1 and Dig out 2.
 i am feeding 12v to pin 2 (pwr 1)  and gnd to pin 1. on the grey connector.
  • So do the dig out 1 and 2 output 12v+ when the button is pressed?
  • do i also need to add 12v to Pwr 2, Pwr 3 and Pwr 4 too?
[/li]
[/list]

many thanks.
4
Displays / Re: DM430 new hardware file
« Last post by Tor on March 29, 2023, 10:57:47 AM »
Hello,

We got some question about this HWD.
Due to some issues the HWD was pulled back from the PLUS+1 Update Center. I don't have any information when this will be released again.

I'm sorry about that.
5
Controllers / SC050_C1P46_Status_128_Problem
« Last post by macbahi on March 28, 2023, 04:01:23 PM »
Hi,

Any controller I use (Sc024 or SC050) to set ON coil using digital output as C1P46 to controller give me error C1P46 status=128 as showing in picture.
I must to reset the controller even though the output was set off. And the current was correct around 1,4A.
The error occurring after a few minutes that everything was working fine. Sometimes the error appears in a little time and sometimes more time.
Coil is sun 770-214  14V  8.9Ohm   and DIN connector S18209TC411.

Please where is the problem?

Thank you very much
With best regards
6
PLUS+1 GUIDE CANKing / Re: Hex Mode
« Last post by FluidPowerTom on March 27, 2023, 05:27:38 PM »
Tor, you're the man.  I wish I'd asked this years ago...

Edit:  Oh wait, never mind.  Okay, I'm actually clicking that 'Options' button, and nothing is coming up.  I tried going on bus with the virtual CG150, and still nothing pops up.

Even so, if I go to the Options dropdown in the main windows and click Global that pops up a window called Program Options.  It really would seem like selecting hexadecimal in that window would change the output window as well.  Why would it only change the window for putting together messages to transmit but not the output window?  I mean the area it's in is Options->Global.  There's nothing about that which makes it look like it's only for the message creation.

Edit 2:  Okay I figured it out.  You have to click to highlight Standard Text Format in that lower part of the window and then click options.  Pretty clunky.  Still I would think that the Options->Global window pop up would do the same thing.
7
Controllers / SC050-120 Safety Layer Issue
« Last post by acmall on March 27, 2023, 03:27:21 PM »
I am getting reports of an intermittent issue on a SC050-120 with a Safety Layer Failure. The SafetyLayer.Failure signal has bit 4 set. I can't find any information on this other than the description of ISR Monitor Error, I am guessing ISR stands for Interrupt Service Routine. It is mostly happening at power on and needs a power cycle to clear.

Has anyone seen this before?

8
General controls / Re: Error 448
« Last post by Daan on March 27, 2023, 03:17:57 PM »
Hey mvanwiechem

It was a problem with the permissions of the IT service. I've been working on a virtual computer ever since so I don't have this problem anymore.

Still, thanks for your time!
9
General controls / Re: Error 448
« Last post by mvanwiechen on March 27, 2023, 03:01:47 PM »
Is your project/folder located on a Network drive?  Sometimes this can cause issues with compiling, and no real error is given.

Try to copy your project to C drive, and see if you get the same error.
10
PLUS+1 GUIDE CANKing / Re: Hex Mode
« Last post by Tor on March 27, 2023, 08:20:10 AM »
Hello FluidPowerTom.

It was a while since I used CAN King and I'm not an expert, but I guess both of the things you ask for is possible.

1. Hexadecimal in the output window. 
See page 1 in the CAN King pdf.

2. Cyclic messages.
See page 2 - 5 in the CAN King pdf.
You need to have a message (History List) to create a cyclic transmission (Timed Transmission).  I included the One-Shot messages as a bonus.

I hope I understood your question correct and that this helped.

Have a nice day.
Pages: [1] 2 3 ... 10