Author Topic: DP600 Multi Input?  (Read 4809 times)

kidproquo

  • Guest
DP600 Multi Input?
« on: April 10, 2012, 10:29:44 PM »
Hi,

Page 10 of the Technical Information document (520L0699) shows a pin-out for the DP600 that shows pins 9 and 10 to be Multi-Inputs. Is this correct? Page 9 has a different pin-out configuration for the same 12-pin connector.

Regards,
Kid

Offline hproffitt

  • PLUS+1 Developer
  • ***
  • Posts: 28
  • Karma: +0/-0
Re: DP600 Multi Input?
« Reply #1 on: June 29, 2012, 08:23:48 PM »
It would appear that page 10 is a bit misleading, or possibly even a typo.  I went into the most recent templates of the 600, 610, & 620 and all use these pins strictly as digital in for an encoder input.  I'm not sure why theses pins couldn't be used as just digital ins if need be, but I haven't read through the entire API on it yet; so I may be missing something in there.