PLUS+1 Hardware > PLUS+1 Compliant Hardware
PVED-CC PLUS+1 GUIDE
dlewis:
I asked this years ago, Does Danfoss have a hwd file or compliance block for the PVED valves to be used in Plus+1 programming. If not do they plan on releasing one?
tkane:
They have a compliance block (i use it), but they have not released it.
FluidPowerTom:
I'm pretty sure that everything that is configurable with the PVED-CC Service Tool is also configurable with GUIDE from a MC. That said, a lot of it may require a fair bit of work. When I asked the Helpdesk they had not yet been trained to support these, but they'll be able to refer you to somebody internally who can support it.
glouw:
Hi all,
Am I able to change PVED-CC node-IDs? Turns out the node-IDs of the the seven PVED-CC's we own are defaulted to 0x80 (d128).
EDIT:
The PVED-CC's do not show up as ECU's in the PLUS+1 GUIDE Service Tool. We're able, however, to write AVC messages and read AVEF messages from the PVED-CC. CANKing verifies this.
PS. The valves are not hooked up to hydraulic lines. Do they require a pilot pressure to become operational?
George:
--- Quote from: glouw on April 13, 2015, 08:20:33 PM ---Hi all,
Am I able to change PVED-CC node-IDs? Turns out the node-IDs of the the seven PVED-CC's we own are defaulted to 0x80 (d128).
EDIT:
The PVED-CC's do not show up as ECU's in the PLUS+1 GUIDE Service Tool. We're able, however, to write AVC messages and read AVEF messages from the PVED-CC. CANKing verifies this.
PS. The valves are not hooked up to hydraulic lines. Do they require a pilot pressure to become operational?
--- End quote ---
Hi Glouw,
Make sure to activate the WEBGPI- PVED-CC protocol. (CTRL+ALT+P)
If you're missing this protocol I suggest you download the latest service tool (7.1.10 or later)
I've lost a whole day to figure this out, since this isn't documented, and I was to stubborn to search help elsewhere
EDIT: To make matters worse, the tool on the Danfoss website includes service tool 7.0.6 which hasn't got the needed protocol!
Shame on you, Danfoss :p
Best Regards
George
Navigation
[0] Message Index
[#] Next page
[*] Previous page
Go to full version