PLUS+1 Hardware > PLUS+1 Compliant Hardware
PVED CC
Rafal_Typiak:
I've downloaded it and installed but I can't seem to get it to work with my PVED-CCs. Service Tools can't find the valves when I scan the system (it never did, even with the elder versions of ST) and it seems that this is a necessity to actually do anything. Does that mean I have an older versions of the PVED-CCs and will not be able to work with them using the ST pages?
glouw:
It's 2015 now, which is about four years after the post above, so here's to a massive necro-bump.
I'm having the same problem. I'm to change the NODE-ID of our PVED-CC's but the PVED-CC's do not show in the Service Tool. Does anyone know of a way to use PLUS+1 GUIDE with a CAN Transmit and Receive block and an MCU to change the NODE-ID? Is this possible?
George:
the PVED CC Diagnostic file will help, once you get it communicating
To get so far, You need the tool
http://powersolutions.danfoss.com/workarea/downloadasset.aspx?id=17179901358
But don't use the included Guide Service tool. Download the latest 7.1.11, because the 7.0.6 included misses a needed communication Protocol
After installing the Guide Service tool 7.1.11 open the PVED CC Diagnostic_2014.p1d, and enable the protocol "WebGPI PVED CC" (CTRL+ALT+P)
Now you'll be able to connect to the PVED CC. I would suggest to connect to one at a time to set the address first
Best regards
Geert
glouw:
Thanks, George.
Continued here for others interested: http://www.plus1forum.danfoss.com/index.php?topic=747.0
Navigation
[0] Message Index
[*] Previous page
Go to full version