PLUS+1 Software > Function Library
TSC1 SPN4206; 4207
spittet:
I want to add to this thread.
We tried controlling engine speed on a Hatz 4H50TIC engine which is Tier4 Final. We used the TSC1_TX1 block v3.00 from Danfoss. The engine responded to engine speed request change up to 1200 RPM. More than that and the the engine returns at idle with a SPN1108 engine code.
As stated above, the solution was to set the CANData_7 at 0xFF instead of the variable checksum.
To do it, we build a custom TX message, but it would be nice if the TSC1_TX1 block could be updated so that this checksum can be set ON or OFF.
Sam
Nilla:
Hello Spittet!
There is a later released version 3.03 from July 2015, have you tried that? If you have and still have the same problem please send your project and problem description to plus1helpdesk@danfoss.com so that we can investigate it.
Best regards,
Nilla Troedsson
PLUS+1 Helpdesk
pinias:
Hey guys,
did you solve your issue?
I am trying to set engine RPM of an FPT TIER4 engine but it seems to ignore my request.
I am using the TSC1 V5 of Danfoss it comes with the checksum choice but still the mesage is not taken by the engine ECM
has anyone used the latest TSC1 V5 from danfoss in a Tier4 engine, ?
if so, what were your settings?
thanks
Navigation
[0] Message Index
[*] Previous page
Go to full version