PLUS+1 Hardware > Controllers
Low current draw
(1/1)
paterianus:
I'm getting faults on two digital outputs on a MC50-20 driving IDEC RJ1S-C-D24 relays. Am I not drawing enough current to let the controller know its not an open circuit, if so what is the current needed to fake the system?
brianbassett:
Look at note 5 on the Application Interface Document for the MC050-20.
Basically you need at least 500mA to guarantee that a open load error will not occur.
paterianus:
1/2 amp, is pretty big draw, not to mention the 12watts.
Navigation
[0] Message Index
Go to full version