Author Topic: Update CS10 Hdw file  (Read 21001 times)

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 110
  • Karma: +2/-0
    • Getman Corporation
Update CS10 Hdw file
« on: August 11, 2022, 08:26:42 PM »
How long should it take to download a new program into a CS10 when going from Hwd version 257 to version 303?  So far it's taking what feels like an eternity.

Offline FluidPowerTom

  • PLUS+1 Guru
  • *****
  • Posts: 363
  • Karma: +33/-0
Re: Update CS10 Hdw file
« Reply #1 on: December 06, 2022, 07:08:34 PM »
I just did it last week, and it took over an hour.  Helpdesk said it was normal
Controls Engineer
Hydra-Power Systems

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 301
  • Karma: +28/-1
Re: Update CS10 Hdw file
« Reply #2 on: December 07, 2022, 11:05:39 AM »
Hello,

I'm not an CS expert, so don't quote me on this.

When you change the HWD in a CS product, you also replace the LINUX OS, like in the DM1x00. If you use the CG150 as gateway it will take time. A long time.
You should be able to use WiFi, which is faster (nothing I have done myself, but I heard it takes around 2 minutes).
I'm not sure what happens after the update, if you just can connect with WiFi again or if you need to connect with CG150 and change some settings??
 

Here's a video about the CS10 and WiFi connection: https://youtu.be/fV2DmM28Pro

Have a nice day.


Best regards,
Tor
PLUS+1® SW PAE Team