Author Topic: DP700 BusOn  (Read 2620 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 113
  • Karma: +1/-0
DP700 BusOn
« on: August 27, 2021, 12:04:23 AM »
Hi!!
I had BusOff and the red led blinking.
It was done because the can cable was damaged.
I make new cable but the red led stay blinking.

My question is't possible to make BusOn without restart Display.

Thanks
Mac


Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: DP700 BusOn
« Reply #1 on: August 27, 2021, 08:29:10 AM »
Hello macbahi,

When the controller goes to BusOff it tries to reset itself a number of times (5 times is default).
This number can be set in the Unit_Config block in the application template. You can also add a manual reset signal, in addition to the existing one. Read the API before before doing this.

If you don't have a manual reset signal you need to restart the unit.

Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team