Author Topic: SC050_C1P46_Status_128_Problem  (Read 1151 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 113
  • Karma: +1/-0
SC050_C1P46_Status_128_Problem
« on: March 28, 2023, 04:01:23 PM »
Hi,

Any controller I use (Sc024 or SC050) to set ON coil using digital output as C1P46 to controller give me error C1P46 status=128 as showing in picture.
I must to reset the controller even though the output was set off. And the current was correct around 1,4A.
The error occurring after a few minutes that everything was working fine. Sometimes the error appears in a little time and sometimes more time.
Coil is sun 770-214  14V  8.9Ohm   and DIN connector S18209TC411.

Please where is the problem?

Thank you very much
With best regards