PLUS+1 Hardware > PLUS+1 CS Hardware
Update CS10 Hdw file
(1/1)
dlewis:
How long should it take to download a new program into a CS10 when going from Hwd version 257 to version 303? So far it's taking what feels like an eternity.
FluidPowerTom:
I just did it last week, and it took over an hour. Helpdesk said it was normal
Tor:
Hello,
I'm not an CS expert, so don't quote me on this.
When you change the HWD in a CS product, you also replace the LINUX OS, like in the DM1x00. If you use the CG150 as gateway it will take time. A long time.
You should be able to use WiFi, which is faster (nothing I have done myself, but I heard it takes around 2 minutes).
I'm not sure what happens after the update, if you just can connect with WiFi again or if you need to connect with CG150 and change some settings??
Here's a video about the CS10 and WiFi connection: https://youtu.be/fV2DmM28Pro
Have a nice day.
Navigation
[0] Message Index
Go to full version